Selecting a Measurement Type
The menu selects a measurement type. Most of the measurement types available perform a specific type of demodulation and analysis (Vector and Power Spectrum are examples of measurement types that do not perform demodulation). Digital demodulators (all except Analog Demod) contain a subset of the functionality present in the Vector mode but provide extended functionality for modulation analysis.
Selecting the measurement type is the first step of a two-step process required to configure the VSA to demodulate and analyze a modulated signal. First select the demodulator and then configure the modulation setup parameters. For more information about demodulation setup, see the About Demodulation Setup topic.
Each modulation analysis type requires the indicated option to be licensed
For Floating License users, measurement types are only enabled for use when the appropriate floating licenses are available for checkout. See Checking Out a Floating License for more information.
- (89601B-200/8960120xC/8960120xU) configures the VSA to perform basic vector signal analysis.
-
- Power Spectrum (89601B-SSA/8960120xC/8960120xU: Power Spectrum Measurement)
- Adjacent Channel Power (89601PSMC: Adjacent Channel Power Measurement)
- Spectral Emissions Mask (89601PSMC: Spectral Emissions Mask Measurement)
-
- Analog Demod (89601B-200/8960120xC/8960120xU: Analog modulation analysis)
- Digital Demod (89601B-AYA/89601AYAC "Vector Modulation Analysis": Digital Demodulation)
- Custom IQ (89601B-BHK/89601AYAC: Custom IQ Modulation Analysis)
- Custom OFDM (89601B-BHF/89601BHFC: Custom OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Modulation Analysis)
- Component Test (89601B-BHL/8960120xC/8960120xU: Component Test Measurement)
- Channel Sounding (89601CSDC: Channel Sounding Measurement)
- Flex Frame (89601AYAC: Flex Frame Modulation Analysis)
-
- DVB-S2/S2X (89601DVBC: DVB-S2/S2X Measurement)
- DVB-RSC2 (89601DVBC: DVB-RSC2 Measurement)
-
- GSM/EDGE/EDGE Evolution (89601B-AYA/89601AYAC "Vector Modulation Analysis": GSM Global System for Mobile Communications: Originally developed as a pan-European standard for digital mobile telephony, GSM has become the world’s most widely used mobile system. It is used on the 900 MHz and 1800 MHz frequencies in Europe, Asia and Australia, and the 1900 MHz frequency in North America and Latin America./EDGE Enhanced Data for Global Evolution: A technology that gives GSMA and TDMA similar capacity to handle services for the third generation of mobile telephony. EDGE was developed to enable the transmission of large amounts of data at a high speed, 384 kilobits per second. (It increases available time slots and data rates over existing wireless networks.)/EDGE Evo demodulation)
- W-CDMA (3GPP) /HSPA (89601B-B7N/89601B7NC: Wideband Code Domain Multiple Access (3GPP) vector modulation analysis)
- cdma2000/1xEV-DV (89601B-B7N/89601B7NC: Code Domain Multiple Access 2000 vector modulation analysis)
- TD-SCDMA (89601B-B7N/89601B7NC: 3GPP N-TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. 1.28 Mcps Mega Chip Per Second: A measure of the number of bits (chips) per second in the spreading sequence of direct sequence spreading code. vector modulation analysis)
- 1xEV-DO (89601B-B7N/89601B7NC: 1xEV-DO First Evolution - Data Only vector modulation analysis)
- NB-IoT (89601B-BHT/89601BHTC: NB-IoT Modulation Analysis)
- LTE (89601B-BHD/89601BHGC: LTE FDD Frequency Division Duplex: A duplex scheme in which uplink and downlink transmissions use different frequencies but are typically simultaneous. Modulation Analysis and 89601B-BHE/89601BHHC: LTE TDD Modulation Analysis)
- LTE-Advanced (89601B-BHG/89601BHGC: LTE-Advanced FDD Modulation Analysis and 89601B-BHH/89601BHHC: LTE-Advanced TDD Modulation Analysis)
- 5G NR (89601B-BHN/89601BHNC: 5G NR Modulation Analysis)
- Pre-5G (89601B-BHN/89601BHNC: Pre-5G Modulation Analysis)
- 6GR Modulation Analysis (89601B6GC: 6GR Modulation Analysis)
-
- IEEE 802.11a/g/j/p OFDM (89601B-B7R/89601B7RC: WLAN WLAN - Wireless Local Area Network: A system that includes the distribution system (DS), access points (APs), and portal entities. It is also the logical location of distribution and integration service functions of an extended service set (ESS). A WLAN system contains one or more APs and zero or more portals in addition to the DS. Modulation Analysis)
- IEEE 802.11b/g DSSS/CCK/PBCC (89601B-B7R/89601B7RC: WLAN Modulation Analysis)
- IEEE 802.11n/ac/ax/be (89601B-BHJ/89601BHXC: 802.11n/ac HT high throughput/VHT very high throughput (VHT) physical (PHY) layer protocol data unit (PPDU):A PPDU transmitted using the TXVECTOR FORMAT parameter equal to VHT. OFDM Modulation Analysis and 89601B-BHX/89601BHXC: 802.11ax/be HE/EHT Modulation Analysis)
- IEEE 802.16 OFDM (89601B-B7Y/89601B7RC: IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.16 OFDM(A) Mobile/Fixed WiMAX Modulation Analysis)
- IEEE 802.16 OFDMA (89601B-B7Y/89601B7RC: IEEE 802.16 OFDM(A) Mobile/Fixed WiMAX Modulation Analysis)
- IEEE 802.15.4/4z HRP UWB (89601BHTC: IEEE 802.15.4/4z HRP UWB modulation analysis)
- Bluetooth Demod (89601BLTC: Bluetooth Modulation Analysis)
- Bluetooth Spectrum (89601BLTC: Bluetooth Modulation Analysis)
-
- Pulse (89601B-BHQ/89601BHQC: Configures the VSA to perform pulsed radar measurements)
- FMCW Radar: (89601B-BHP/89601BHPC: Configures the VSA to perform FMCW radar measurements)
- Advanced Radar: (89601BHQC: Configures the VSA to perform continuous wave and pulse radar measurements)
-
- TEDS (TETRA 2) (89601B-BHA/89601AYAC: TEDS (TETRA Trans-European Trunked Radio. A communications system standard. 2) Modulation Analysis)
- RFID (89601B-BHC/89601BHTC: RFID "Radio Frequency Identification" Modulation Analysis)
- MB-OFDM (89601B-BHB/(discontinued): MB-OFDM "MultiBand OFDM" modulation analysis)
- DOCSIS 4.0 Upstream (89601B-BHM/89601BHMC: DOCSIS 4.0 Upstream modulation analysis)
- DOCSIS 4.0 Downstream (89601B-BHM/89601BHMC: DOCSIS 4.0 Downstream modulation analysis)
See Also